MC9S12XDP512 Missing PLL Filter Calculator

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC9S12XDP512 Missing PLL Filter Calculator

606件の閲覧回数
christianpeters
Contributor I

Dear all,

in AN3262  a PLL Filter Calculator is described, but in reality it is for 9S12 an cannot be used for the far faster S12X Family,

Is there an apnote using the PLL Filter with the 9S12X family?

 

Thanks

ラベル(1)
0 件の賞賛
3 返答(返信)

365件の閲覧回数
kef2
Senior Contributor IV

Hi

Can't find source URL, I found attached EXE stored in my datasheets folder.

Edward

0 件の賞賛

365件の閲覧回数
christianpeters
Contributor I

Thank you Edward,

In the calculators window here are the terms “stability factor” and “damping factor”.

As I found no appnote or document for the calculator, may you explain these terms to me?

Kind regards

Christian Peters

Senior Field Application Engineer

EBV GmbH & Co. KG

Im Technologiepark 2-8

85586 Poing

Tel. +49 8121 774 533

Fx. +49 8121 774 540

0 件の賞賛

365件の閲覧回数
kef2
Senior Contributor IV

Stability =50 and damping factor =0.9, I think are things, mentioned XDP512 RM

A.5.3.1 XFC Component Selection

The loop bandwidth fC should be chosen to fulfill the Gardner’s stability criteria by at least a factor of 10, typical values are 50. z = 0.9 ensures a good transient response.


I used default 50 and 0.9 for years without any problems. If I had problems with stability or too slow PLL locking, I would study it deeper/

0 件の賞賛