MC9S12G EEPROM maximum erase and write cycles limitations

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC9S12G EEPROM maximum erase and write cycles limitations

1,764 Views
ramakrishnaredd
Contributor I


I want to know EEPROM limitations can somebody help.

Labels (1)
2 Replies

1,535 Views
RadekS
NXP Employee
NXP Employee

Hi Ramakrishnareddykunta,

Please look at Table A-39. NVM Reliability Characteristics in RM.

http://www.nxp.com/files/32bit/doc/ref_manual/MC9S12GRMV1.pdf

EEPROM number of program/erase cycles (-40°C ≤ Tj ≤ 150°C)  nFLPE  min. 100k; typ. 500k Cycles

EEPROM number of program/erase cycles (150°C ≤ Tj ≤ 160°C)  nFLPE min. 10k; typ. 500k Cycles

NOTE: Spec table quotes typical endurance evaluated at 25°C for this product family. For additional information on how Freescale defines Typical Endurance, please refer to Engineering Bulletin EB619.

http://www.nxp.com/files/microcontrollers/doc/eng_bulletin/EB618.pdf

http://www.nxp.com/files/microcontrollers/doc/eng_bulletin/EB619.pdf

I hope it helps you.

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,535 Views
ramakrishnaredd
Contributor I

Hi Radek Sestak,

Thank you so much for your help...!!

0 Kudos
Reply