MC9S12E128

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,598件の閲覧回数
Fast
Contributor V
What is the MC9s12E256/128/64 for?
Is it a 3phase motor controller, which would explain its high resolution 3pairs PWM, but no CAN or easy up-grade to XGATE part?
Should we move to a DSP type device?
 
 
 
 
ラベル(1)
0 件の賞賛
返信
1 解決策
2,099件の閲覧回数
blood
Contributor III
We use it a general purpose micro (E256) as it has a good number of I/O and it accepts 3V which for us was a major requirement a long with SPI, SCI, ADC and DAC but we didn't need any CAN. Most of the micros have these but the number of each varies between device families. A couple more SPI would have been nice.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,099件の閲覧回数
Nabla69
Contributor V
Hi,

Looks more like a general purpose than specialized.
There's one reference manual for a Uninterruptible Power Supply using S12E.

Alban.
0 件の賞賛
返信
2,100件の閲覧回数
blood
Contributor III
We use it a general purpose micro (E256) as it has a good number of I/O and it accepts 3V which for us was a major requirement a long with SPI, SCI, ADC and DAC but we didn't need any CAN. Most of the micros have these but the number of each varies between device families. A couple more SPI would have been nice.
0 件の賞賛
返信
2,099件の閲覧回数
Fast
Contributor V
CAN is readily added with the Bosch CC770.
The enhanced PWM is also found on the flexray'd 9S12XF, suggesting it has a automotive use. Guessing, could it be for starter/generator?
 
Fast
 
0 件の賞賛
返信