MC9S12DT256, To use an IR demodulator

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MC9S12DT256, To use an IR demodulator

1,431 次查看
IdeaSourcesLLC
Contributor I
Hi all,
 
My goal is to use the MC9S12DT256, as an IR demodulator. I may be at the wrong place, but I am looking for advice on how to tackle this. What would be a idea, would be to find a IR decoder that converts the IR data (from a receiver) into a serial string. I have looked and cannot seem to find any decoder IC's.
 
Since freescale offers many control aplications, I was curious if there are datasheets/appliaction notes anywhere with perhaps some example code, C or asm is fine.
 
Thanks
标签 (1)
0 项奖励
回复
1 回复

684 次查看
mke_et
Contributor IV
I haven't seen that as such, but there are fairly common IR modules that output serial data that you can pick up cheap. I'm not sure if they output bit streams or bytes, but they go a long way to doing the 'IR' portion of the detect and decode.
0 项奖励
回复