MC9S12DT256, To use an IR demodulator

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC9S12DT256, To use an IR demodulator

1,432 Views
IdeaSourcesLLC
Contributor I
Hi all,
 
My goal is to use the MC9S12DT256, as an IR demodulator. I may be at the wrong place, but I am looking for advice on how to tackle this. What would be a idea, would be to find a IR decoder that converts the IR data (from a receiver) into a serial string. I have looked and cannot seem to find any decoder IC's.
 
Since freescale offers many control aplications, I was curious if there are datasheets/appliaction notes anywhere with perhaps some example code, C or asm is fine.
 
Thanks
Labels (1)
0 Kudos
Reply
1 Reply

685 Views
mke_et
Contributor IV
I haven't seen that as such, but there are fairly common IR modules that output serial data that you can pick up cheap. I'm not sure if they output bit streams or bytes, but they go a long way to doing the 'IR' portion of the detect and decode.
0 Kudos
Reply