MC9S12DG128CPVE 5L40K

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC9S12DG128CPVE 5L40K

631 Views
lixinhua
Contributor I

1L59W, 5L40K, 2L94R ,I once used five "5L40K" pieces, all bad, we developed the firmware program in the run process to stop. All change to the new "1L59W", all good, the problem solution. What are the differences between Mask set "5L40K" “2L94R” and "1L59W?

Tags (1)
0 Kudos
2 Replies

457 Views
RadekS
NXP Employee
NXP Employee

Hi Li,

please look at an attached file with the masksets comparison.

I hope it helps you

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

457 Views
kef2
Senior Contributor IV

Hi,

It is not clear from your description which maskset is OK and which is not.

I think you still need to debug your code. Also you should compare erratas for given mask sets, all listed here:

https://www.nxp.com/products/processors-and-microcontrollers/additional-processors-and-mcus/8-16-bit...

Edward

0 Kudos