MC9S12DG oscillator layout confusion

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MC9S12DG oscillator layout confusion

跳至解决方案
1,110 次查看
jpurdom
Contributor I

Hi!

 

I am working to re-layout one of our display cards due to interference issues. I have recently started working on the uP (MC9S12DG128). Reading through  the design guides I have run across conflicting guidelines on how to layout the oscillator circuit. In the uP datasheet and the original hardware design guide it says to leave an 'exclusion zone' under the osc section due to stray capacitance worries. However, in more recent docs (also for the same MC9S12 family) I have found it saying that running a gnd plane under the osc is not a problem and can even be advantageous in noisy environments.

 

Which guideline should I go with? This PCB is mounted in a very noisy environment.

 

Thanks!

 

 

标签 (1)
标记 (3)
0 项奖励
回复
1 解答
996 次查看
RadekS
NXP Employee
NXP Employee

I am afraid that for this topic you will never get “right” answer. Both solution has own advantages and disadvantages. I am not PCB layout expert but from my experience I know that there isn’t any strict rule, just few recommendations.

I would like recommend an 'exclusion zone' under the oscillator section. Of course, the main recommendation is to leave the oscillator section as smallest as possible and as close to the MCU.

If you choose GND plane under oscillator section (crystal, capacitors, PLL filter), I would like recommend create here separate GND area which is connected to main GND plane just in one point = at  VSSPLL pin. If you use for example four layer PCB, this GND area should be presented on all layers (areas are connected by via holes).


在原帖中查看解决方案

0 项奖励
回复
1 回复
997 次查看
RadekS
NXP Employee
NXP Employee

I am afraid that for this topic you will never get “right” answer. Both solution has own advantages and disadvantages. I am not PCB layout expert but from my experience I know that there isn’t any strict rule, just few recommendations.

I would like recommend an 'exclusion zone' under the oscillator section. Of course, the main recommendation is to leave the oscillator section as smallest as possible and as close to the MCU.

If you choose GND plane under oscillator section (crystal, capacitors, PLL filter), I would like recommend create here separate GND area which is connected to main GND plane just in one point = at  VSSPLL pin. If you use for example four layer PCB, this GND area should be presented on all layers (areas are connected by via holes).


0 项奖励
回复