MC9S12C64MFA Port T set up question

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MC9S12C64MFA Port T set up question

跳至解决方案
1,511 次查看
roberthiebert
Senior Contributor I

MC9S12C64MFA, Code Warrior 5.9.0, coding in assembler.

I am setting up Port T but I'm not sure I'm doing it right. Here is what I am trying to accomplish:

PT0 is for PWM control of a solenoid valve.

PT3 is a general purpose output.

PT1,2 4,5,6,7 are all output compare channels. All are under port control with interrupt on compare match enabled. When I load the output compare value I will set the associated pin to the appropriate state. When the match occurs and the interrupt is triggered I will set the pin to the appropriate state in the ISR.

Here is what I have so far:

movb #$FF,DDRT ; All pins outputs

movb #$01,MODRR ; PWM control on PT0, PT1,2,3 on Timer control

movw #$0000,TCTL1 ; All pins under port control

movb #$F6,TIOS ; Output Compare on PT1,2,4,5,6,7

movb #$01,PWME ; PWM control on PT0

 

Should this work?

 

Regards,

Robert

 

0 项奖励
回复
1 解答
1,490 次查看
roberthiebert
Senior Contributor I

My goodness, I sure had that wrong! Thanks so much for the detailed explanation. As soon as I get my PCB finished I'll try that out.

Regards,

Robert

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,452 次查看
yihanef
Contributor I

Game modes and events include team play, survival elimination, and seasonal tournaments planet clicker 3 online.

0 项奖励
回复
1,493 次查看
lama
NXP TechSupport
NXP TechSupport

Hi,

I tried to do it without test. You can compare.

 

If the alternative function (another from GPIO) is enabled it takes precedence over all enable peripherals at pin with less priority. Priority starts from GPIO (the least) in the pin description table.

When you disconnect TIM from pin and you want to control them as output by SW
in the interrupt(not by automatic OC function) then you have to set it as GPIO output mode.

// set ports
PTT = ; // good to set initial value at the pins before
// it is switched from input(default) to output
DDRT = 0xFE; // pin 7,6,5,4, ,2,1 are driven by SW, pin 0 driven by PWM
// pin 3 is also output in GPIO mode

//select pins connections
MODRR = 0B00000001 // TIM,TIM,TIM,TIM, GPIO,TIM,TIM,PWM

// select TIM function
TCTL1 = 0x00; // The TIM is disconnected from pins, value will be set manualy
TIOS = 0xFE // TIM channels 7,6,5,4,3,2,1 in OC function

// Set PWM parameters, period, duty, polarity

....

// Set TIM parameters .. predcaler, period, OC value

....

// enable interrupt for TIM
TIE = 0B11100110; // enable TIM interrupt for channel 7,6,5,4, 2,1

//enable interrupt globally
asm CLI

// Run timer, set debug possibilities, set fast flag clear for TIM
TSCR1 = 0xF0; // TEN-run timer; (TSWAI,TSFRZ)-good to set
// to be able to debug; fast TIM flags clear,x,x,x,x

// Run PWM_0
PWME = 0x01; // run PWM0 at PT0

 

Best regards,

Ladislav

0 项奖励
回复
1,491 次查看
roberthiebert
Senior Contributor I

My goodness, I sure had that wrong! Thanks so much for the detailed explanation. As soon as I get my PCB finished I'll try that out.

Regards,

Robert

0 项奖励
回复