MC9S12C64MFA IOC4 question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC9S12C64MFA IOC4 question

Jump to solution
3,470 Views
roberthiebert
Senior Contributor I

Hi All,

MC9S12C64, Code Warrior 5.9.0, coding in assembler.

I've been wrestling with a problem I am having getting the input capture function to work for well over a week now with no success. It's time to swallow my pride and beg for help.

I have all the other timer functions working well, but the IC has me stumped, both IOC4 and IOC5. I put together an absolute minimum test code (attached).

If anyone can offer suggestions I'd really appreciate it.

Regards,

Robert

0 Kudos
Reply
1 Solution
3,164 Views
roberthiebert
Senior Contributor I

Hi Daniel,

Update. After trying just about every combination of everything I could think of I finally got the test program to work. I think the key issue was the way I was clearing the flags. As for the IRQ, I didn't notice that the pullups for Port E are set after reset. I used an external pullup in my other program so that kind of messed me up. I've attached my latest test program. Now I have to see if I can get them to work in my main program, but at least I have this working for an example. 

Thanks so much for all your help. I doubt that I could have solved this without it.

Regards,

Robert

View solution in original post

14 Replies
3,458 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Robert,

Can you please first make sure there is an edge at the pin?

Removing the 5V from the pin does not mean there is 0V.

danielmartynek_0-1735901277177.png

 

Regards,

Daniel

0 Kudos
Reply
3,446 Views
roberthiebert
Senior Contributor I

Hi Daniel,

Thanks so much for your prompt response. What you say makes sense to me. I'll modify my board and let you know the results.

Regards,

Robert

0 Kudos
Reply
3,441 Views
roberthiebert
Senior Contributor I

That doesn't appear to be the problem. I tried applying a 5 volt 100mS square wave to PT4 and PTM4 is still not toggling. Have I got my set up correct?

Regards,

Robert

0 Kudos
Reply
3,413 Views
roberthiebert
Senior Contributor I

Hi Daniel,

The fact that my set up looks good is very encouraging. You've made some very good troubleshooting suggestions and I give them all a try. Thanks again.

Regards,

Robert

 

0 Kudos
Reply
3,393 Views
roberthiebert
Senior Contributor I

Hi Daniel,

I'm a bit confused about the PWM and TIM functions and which pins they are assigned to. Should I be checking the PTIP register, the PTIT register or both. At this point it looks like IOC4 is not generating an interrupt but it definitely has a 5 volt square wave signal to the IOC4 pin. I discovered this by placing a break point in the ISR with the debugger, but the program never got there.

On another matter, I could use the IRQ, or XIRQ pin to monitor my external signal but I'm not clear on how to set it up. Could you advise me on this please?

Regards,

Robert

Robert

0 Kudos
Reply
3,379 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Robert,

I'm sorry, it is PTIT.

danielmartynek_0-1736430061988.png

danielmartynek_1-1736430157234.png

 

IRQ/XIRQ example attached

 

 

0 Kudos
Reply
3,355 Views
roberthiebert
Senior Contributor I

Hi Daniel,

I'm not fluent in "C" but I believe the MC9S12C64 IRQ is on Port E1 and XIRQ is on Port E0, not Port B, as your attachment indicates. I didn't bring out PE0 on my board so I am just trying to get the IRQ pin working.

I wrote a new test program to test the IRQ, IOC4 and IOC5 (attached). It is about as brief as I could make it. I have the ITR toggle PTM5 every 100mS. I use this as a trigger to test the input capture ISRs. I have checked the signal at the ISR inputs with a scope and it is a nice clean 5 volt square wave. When I read PTIT is just shows pins 7 and 6 high which is legitimate as they are commanded high in the timer set up. At no point do they indicate high for IOC4 or IOC5. When I put a break point in any of the ISRs the program doesn't get there which indicates to me that the ISRs have not been triggered. Can you offer any suggestions as to what I am doing wrong?

Regards,

Robert

 

0 Kudos
Reply
3,313 Views
roberthiebert
Senior Contributor I

Hi Daniel,

I tried running another larger program I am working on that uses IOC5. It gets a pulsed 5 volt signal to the main board where it is inverted. IOC5 has a pullup and the pulse pulls IOC5 low. I have confirmed this with a scope. With this signal I can also use jumpers to test IOC4 , PE0 (XIRQ) and PE1 (IRQ). I have confirmed continuity of the input pins on the board to the pins on the processor. Even though I have a good signal at the board I'm not able to read it in the ports on the debugger, stopped or running. PTT and PTIT read the same, %11100000. This makes sense because pins 7 and 6 are initialized high and not changed in the program. Pin 5 has a pullup.  A change in IOC4 or IOC5 is not indicated with a pulsed input. When I read PORT E, it is always %00001111. So PE0 and PE1 are always high, no matter what the signal to the board pin is. This indicates to me that there could be an internal problem in the processor, but it seems odd that it should affect these four pins. All the other timer functions work fine, as well as the ITR and ADC channels. Is there any other way I can confirm if these pins are damaged or not?

Regards,

Robert

0 Kudos
Reply
3,247 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Robert,

There is one issue in the code I overlooked.

It is the BSET instruction used to clear the flags.

danielmartynek_0-1736778111352.png

BSET does read-modify-write operation at the register, which clears every flag that is set in the register.

It is explained here:

https://www.nxp.com/docs/en/application-note/AN2554.pdf

 

Can you test it?

 

Thank you,

Daniel

 

 

0 Kudos
Reply
3,233 Views
roberthiebert
Senior Contributor I

Hi Daniel,

Thanks for that link. I studied it and think I have made the correct changes to my program (attached). Unfortunately I still can't get either IOC channel or IRQ to trigger their respective ISRs.

I'm still not quite clear on the IRQ channels. It is my understanding that IRQ (PE1) is set to falling edge capture only if IRQCR, IRQE is set to 1. To enable PE1 does IRQCR, IRQEN have to be set to 1 as well? I tried that and still didn't get it to work.

Is PE0 a separate IRQ channel and if so what triggers it, Falling edge, Rising edge or Hi or Lo level? The manual doesn't give me much information on this, or at least I can't find it if it does.

Regards,

Robert

0 Kudos
Reply
3,204 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Robert,

I believe this is well explained here:

danielmartynek_0-1736863599679.png

https://www.nxp.com/docs/en/data-sheet/MC9S12C128V1.pdf

 

Can you double-check the part ID in the PARTIDH and PARTIDL registers?

danielmartynek_1-1736863920884.png

 

Thank you

 

 

0 Kudos
Reply
3,187 Views
roberthiebert
Senior Contributor I

Hi Daniel,

Thanks for the clarification on IRQ and XIRQ. I think I understand it now. I have experimented with use of the pullup but I still can't get it, or IOC4 or IOC5 to trigger their respective ISRs.

PARTIDH is $31, PARTIDL is $03. What does that tell you?

Regards,

Robert 

0 Kudos
Reply
3,165 Views
roberthiebert
Senior Contributor I

Hi Daniel,

Update. After trying just about every combination of everything I could think of I finally got the test program to work. I think the key issue was the way I was clearing the flags. As for the IRQ, I didn't notice that the pullups for Port E are set after reset. I used an external pullup in my other program so that kind of messed me up. I've attached my latest test program. Now I have to see if I can get them to work in my main program, but at least I have this working for an example. 

Thanks so much for all your help. I doubt that I could have solved this without it.

Regards,

Robert

3,412 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @roberthiebert,

I have gone through the project but I haven't spotted anything wrong in the configuration.

Can you double check all the registers in the debugger's register view?

And instead of just checking the PTM4, read the interrupt flag of the TIM_4 channel.

Also, The PTIP register will give you the state of the pin in any mode.

 

 

0 Kudos
Reply