MC9212XEQ512 - SCI does not work after COP reset

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC9212XEQ512 - SCI does not work after COP reset

2,465 Views
JohnBarber
Contributor II

Hi,

I'm using a MC9212XEQ512 and performs a COP reset by writing to the ARMCOP register:

/* Activate watchdog */COPCTL = 0x07;/* Write wrong value to COP-timer (will cause a reset) */ARMCOP = 0xFF;

 

After reset, the SCI is configured. But nothing is transmitted when I try to.

 

But if I connect my P&E debugger, it works. I.e the SCI transmission is performed.

 

Can someone explain this?

 

/John

Labels (1)
0 Kudos
Reply
4 Replies

1,593 Views
JohnBarber
Contributor II

Edit:

 

I can verify that the SCI is configured correct. I can perform a transmission by directly writing to the data register.

But transmission using TX interrupt does not work without the debugger connected.

/John

0 Kudos
Reply

1,593 Views
J2MEJediMaster
Specialist I

It is possible that you are failing to initialize something that the interrupt hander requires, and the debugger happens to initialize this properly when you are using it. Have you tried one of the example code programs with an interrupt handler and see if it works? If it does, you can compare the example code to your own to see if you can spot the problem.

 

---Tom

0 Kudos
Reply

1,593 Views
JohnBarber
Contributor II

Hi,

the situation is like this:

I have a bootloader that sets up the interupts. This works fine. The bootloader starts executing and I download an application. The application is then started and works fine. Interrupts works too. From the application I then perform a watchdog reset and the bootloader starts again. This time the SCI interupts are note working when the debugger is disconnected. If I have the debugger connected everything works.

 

This is strange.

/John

 

 

0 Kudos
Reply

1,593 Views
J2MEJediMaster
Specialist I

There have been similar situations like yourt reported on these boards. Take a look at this forum https://community.freescale.com/message/56738#56738 and see if it might help you.

 

---Tom

0 Kudos
Reply