Do you have multiple build targets or do you use the change wizard to switch?
With multiple build targets, files can be individually included. Sounds like for the P&E build target one of
the source files is not part of the build. In the project view, in the files tab, there is a column to configure this, its only visible if
there are multiple build targets.
Which kind of symbols are missing? Symbols defined in your code?
Daniel