LIN tesing on DEMO9S12XDT512

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LIN tesing on DEMO9S12XDT512

2,897 Views
tranvkhoa
Contributor I
Hello everybody

I have bought DEMO9S12XDT512 from Freescale, now I want to test LIN
communication between these boards but I cannnot find LIN driver for
this kind of MCU. Could you please help?

Thanks,
Khoa
Labels (1)
0 Kudos
Reply
5 Replies

959 Views
Alban
Senior Contributor II
Hello,
 
You should start by searching in the product page.
 
 
It gives pertinent entries like:
AN2732
Using XGATE to Implement LIN Communication on HCS12X  
Others are also available there.
Regards,
Alban.
0 Kudos
Reply

959 Views
tranvkhoa
Contributor I
Dear Alban

Thanks for your reply. Is there any software for AN2732? I cannot find one.

Thanks,
Khoa
0 Kudos
Reply

959 Views
J2MEJediMaster
Specialist I
The listing for the driver is within the file. I have searched and don't see a separate file that contains the software.

---Tom
0 Kudos
Reply

959 Views
BuiHieu
Contributor I
Dear Mr.Alban,
       I have read AN2732 carefully, but I can't know how to use those codes inside. Could you please explain to me more detail? Please sent to me an example code if you have.
      Thanks you alot!
Ngoc Hieu
 
0 Kudos
Reply

959 Views
Alban
Senior Contributor II
Hello,

Information on how to use the XGATE library is located in the following document:

AN3145 
XGATE Library: Using the Freescale XGATE Software Library

Regards,
Alban.
0 Kudos
Reply