LIN conformance report -MM912H634CV1AE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LIN conformance report -MM912H634CV1AE

4,446 Views
amit1234
NXP Employee
NXP Employee

Hi

   Pls help to share LIN conformance report for MM912H634CV1AE.

 

Thanks,

Amit Gombi

0 Kudos
Reply
4 Replies

4,339 Views
jrrlopez
NXP Employee
NXP Employee

Hi Amit,

Just to give you an update, this search has continued internally and it has been clarified that for this device two tests were performed. For LIN phy conformance to the ISO spec, it was done through C&S. For the EMC conformance testing, it was done through IBEE Zwickau. As soon as that information is obtained we will share it.

Thanks,

Juan

 

0 Kudos
Reply

4,234 Views
jrrlopez
NXP Employee
NXP Employee

Hi Amit,

As an additional update, our internal search has concluded and we haven't been able to find that report internally (it previously belonged to another product line and that information is not available on their end).  This has taken longer than what we anticipated.

We will contact the corresponding test houses (C&S and also IBEE Zwickau) to request them to please share those reports with us. We will keep you posted with any update.

Thanks,

Juan

 

0 Kudos
Reply

4,213 Views
jrrlopez
NXP Employee
NXP Employee

Hello Amit,

We've now obtained the conformance test reports for LIN/SAE. Please find them on the link here

Thanks,

Juan

 

0 Kudos
Reply

4,391 Views
jrrlopez
NXP Employee
NXP Employee

Hello Amit, apologies for the delay responding, but can you please clarify which type of LIN conformance testing report is required? As as reference you can find examples from S12 MagniV devices on the link here. As you can see they basically cover:

  • Static/dynamic Electrical conformance to the LIN spec (voltages, timings) - covered by a company called C&S.
  • EMC conformance to certain car OEM requirements - covered by labs like IBEE Zwickau or Mooser.

Since this device is quite old, we're searching internally to see which kind of tests were performed back then. We will come back to you once we find more information.

Thanks,

Juan

 

0 Kudos
Reply