I really don't know where these definitions come from.
Can someone explain why segment FFFA of 6 bytes overlaps segment FFFE of 2 bytes?
Not that I can't count, but I don't know why the Processor Expert defined these two segments on the same space.
Which peripheral did I add that caused PE to define ivVreset at 0xFFFE? None of the peripheral definitions mention this address. However, the definition shows up in Vectors.c which is generated by PE.
/*lint -save -e950 Disable MISRA rule (1.1) checking. */
static const tIsrFunc _ResetVectorTable[] @0xFFFAU = { /* Reset vector table */
/*lint -restore Enable MISRA rule (1.1) checking. */
/* Reset handler name Address Name Description */
&_EntryPoint, /* 0xFFFA ivVcop unused by PE */
&_EntryPoint, /* 0xFFFC ivVclkmon unused by PE */
&_EntryPoint /* 0xFFFE ivVreset used by PE */
};
It looks like 0xFFFA is ResetVectorTable
I just don't know how to fix this.
解決済! 解決策の投稿を見る。
Hello
There might be some special bean that you have added to your project and that creates this additional
table.
void (* near const _vect[])() @0xFFFE = { /* RESET Interrupt vector */
_Startup |
};
I am unable to reproduce that locally, so I would recommend you to submit a service request through our on line support web page for that.
Click here to submit a Service Request.
Make sure to attach a project reproducing the trouble.
CrasyCat
There is also this definition ...
extern near void _Startup(void); | /* reset interrupt service routine */ |
void (* near const _vect[])() @0xFFFE = { /* RESET Interrupt vector */
_Startup |
};
Can I move this to another location?
How would I do that? Which address is appropriate for Startup?
Hello
I would recommend to delete the lines:
void (* near const _vect[])() @0xFFFE = { /* RESET Interrupt vector */
_Startup |
};
If you are building a Processor Expert application you should let Processor Expert handle the generation of the vector table.
The application entry point for a Processor Expert generated application is _EntryPoint. This function initializes some hardware devices and then calls _Startup.
CrasyCat
Thanks, but the problem with that is that ALL of the code was generated by Processor Expert and it will overwrite that change the next time I run make.
Is this a bug in PE maybe?
I am too new to CodeWarrior.
Hello
There might be some special bean that you have added to your project and that creates this additional
table.
void (* near const _vect[])() @0xFFFE = { /* RESET Interrupt vector */
_Startup |
};
I am unable to reproduce that locally, so I would recommend you to submit a service request through our on line support web page for that.
Click here to submit a Service Request.
Make sure to attach a project reproducing the trouble.
CrasyCat