Is the same die in 9S12ZVC 48 pins and 64 pin?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Is the same die in 9S12ZVC 48 pins and 64 pin?

跳至解决方案
1,254 次查看
Snaku
Contributor III

Hi,

I am initializing unused pins on 9S12ZVC wih 48 pins package, does anyone know there are non-bonded pins of the die? Does it use the same die with 64 pins package?

Thank you,

Snaku

标签 (1)
0 项奖励
回复
1 解答
1,076 次查看
lama
NXP TechSupport
NXP TechSupport

Hi,

There is only one mask set of this device available in recent time. The mask set is 0N23N. Mask set defines die features and corresponding errata.

The answer is in this case is yes. They have the same die. In the future, if there is also another mask set available, then the die will be different with a new errata list.

Best regards,

Ladislav

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,077 次查看
lama
NXP TechSupport
NXP TechSupport

Hi,

There is only one mask set of this device available in recent time. The mask set is 0N23N. Mask set defines die features and corresponding errata.

The answer is in this case is yes. They have the same die. In the future, if there is also another mask set available, then the die will be different with a new errata list.

Best regards,

Ladislav

0 项奖励
回复
1,076 次查看
Snaku
Contributor III

Hi Ladislav,

Thanks for your quick response.

Snaku

0 项奖励
回复