Is the same die in 9S12ZVC 48 pins and 64 pin?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is the same die in 9S12ZVC 48 pins and 64 pin?

ソリューションへジャンプ
1,251件の閲覧回数
Snaku
Contributor III

Hi,

I am initializing unused pins on 9S12ZVC wih 48 pins package, does anyone know there are non-bonded pins of the die? Does it use the same die with 64 pins package?

Thank you,

Snaku

ラベル(1)
0 件の賞賛
返信
1 解決策
1,073件の閲覧回数
lama
NXP TechSupport
NXP TechSupport

Hi,

There is only one mask set of this device available in recent time. The mask set is 0N23N. Mask set defines die features and corresponding errata.

The answer is in this case is yes. They have the same die. In the future, if there is also another mask set available, then the die will be different with a new errata list.

Best regards,

Ladislav

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,074件の閲覧回数
lama
NXP TechSupport
NXP TechSupport

Hi,

There is only one mask set of this device available in recent time. The mask set is 0N23N. Mask set defines die features and corresponding errata.

The answer is in this case is yes. They have the same die. In the future, if there is also another mask set available, then the die will be different with a new errata list.

Best regards,

Ladislav

0 件の賞賛
返信
1,073件の閲覧回数
Snaku
Contributor III

Hi Ladislav,

Thanks for your quick response.

Snaku

0 件の賞賛
返信