Is the same die in 9S12ZVC 48 pins and 64 pin?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is the same die in 9S12ZVC 48 pins and 64 pin?

Jump to solution
1,527 Views
Snaku
Contributor III

Hi,

I am initializing unused pins on 9S12ZVC wih 48 pins package, does anyone know there are non-bonded pins of the die? Does it use the same die with 64 pins package?

Thank you,

Snaku

Labels (1)
0 Kudos
Reply
1 Solution
1,349 Views
lama
NXP TechSupport
NXP TechSupport

Hi,

There is only one mask set of this device available in recent time. The mask set is 0N23N. Mask set defines die features and corresponding errata.

The answer is in this case is yes. They have the same die. In the future, if there is also another mask set available, then the die will be different with a new errata list.

Best regards,

Ladislav

View solution in original post

0 Kudos
Reply
2 Replies
1,350 Views
lama
NXP TechSupport
NXP TechSupport

Hi,

There is only one mask set of this device available in recent time. The mask set is 0N23N. Mask set defines die features and corresponding errata.

The answer is in this case is yes. They have the same die. In the future, if there is also another mask set available, then the die will be different with a new errata list.

Best regards,

Ladislav

0 Kudos
Reply
1,349 Views
Snaku
Contributor III

Hi Ladislav,

Thanks for your quick response.

Snaku

0 Kudos
Reply