Is it necessary to use PDO and PDOCLK for debugging and downloading the S912ZVML32F3MKH chip program

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is it necessary to use PDO and PDOCLK for debugging and downloading the S912ZVML32F3MKH chip program

902件の閲覧回数
yankui666
Contributor III

I am using the S912ZVML32F3MKH chip. If I don't use the PDO and PDOCLK pins and only use BKCD, RST, GND, and VDDX, can I debug and download the program properly. Do PDO
and PDOCLK require a download port to debug the download program?

0 件の賞賛
返信
2 返答(返信)

872件の閲覧回数
lama
NXP TechSupport
NXP TechSupport

Hi,

 

We recommend using all the necessary pins so that all debugging functions are available. You don't know if you'll ever need it and then you'll miss it. For example, the trace function. In addition, the debugger can have a property implemented when it needs these pins. We don't see it because it is given by the implementation of the debug interface, its protocol and properties, which is not our product. Of course, if you check your specific usage, then the possibility is there, but as I already wrote, it is better to use the full interface.

Best regards,

Ladislav

0 件の賞賛
返信

27件の閲覧回数
emilio
Contributor I
If I have the Multilink ans Codewarrior, how can I download the firmware?, any sample project or documentation related, how can I do?
I am try to use BKCD, RST, GND, and VDDX.
0 件の賞賛
返信