In what condition Flash SW image get erased/corrupted is S12 Microcontroller

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

In what condition Flash SW image get erased/corrupted is S12 Microcontroller

1,186 Views
KKumar
Contributor II

Hi NXP,

We have application SW written from S12 Microcontroller for our project and observed that in some of the microcontroller on PCB the application SW is not present after flashing to it.

We want to know in what condition this application SW gets erased or corrupted from flash memory.??

 

 

 

0 Kudos
Reply
3 Replies

1,172 Views
KKumar
Contributor II

Hi @lama 
Thanks for your quick response

I was wondering, Does any high spikes/voltage on any of the microcontroller pin effect flash memory(Corrupt)??

 

Regards

Kishore

0 Kudos
Reply

1,134 Views
lama
NXP TechSupport
NXP TechSupport

Hi,

I am sorry I have missed your response.
It can happen anything in the case of voltage spices. There is a lot of theory in electronics what  overvoltage or overcurrent can cause. Each spike over the operating characteristics is usage the device out of operating characteristics and you should thing about circuitry which filters these spikes.
Otherwise there is no guaranty from NXP side.


Best regards,

Ladislav

0 Kudos
Reply

1,180 Views
lama
NXP TechSupport
NXP TechSupport

Hi,

Possible issues…

 

- Reset while flashing … some  SBC or anything

- Incorrect Flash clocks … good to check also bus clock

- The MCU is secured…suggest t mass erase entire memory and then write unsecure bits because if they are not set to unsecure state then any reset secures the MCU.

- The MCU is secured after loading the code. It is not possible to read the code from outside but it should be normally executed.

 

Best regards,

Ladislav

0 Kudos
Reply