I2C IBSR_IBB clearing early

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I2C IBSR_IBB clearing early

2,138 次查看
sricker
Contributor I
CW Pro v4.6
9S12DT256, mask 0L01Y
 
What would cause the IBB bit in IBSR to clear in the middle of a byte being transmitted?
 
I am trying to write to and then read and expansion port chip. I had been writing successfully but when I started to do the reads I noticed that my I2C bean function CheckBus() which is a macro for IBSR_IBB is clearing in the middle of a byte being transmitted. Because the RecvBlock function takes a pointer to a buffer I was calling that function and then trying to wait for the indication that a specified number of bytes had been received.
 
I need to write to the expansion port chip one byte address with write bit set and the number of the register to read as the second byte. Then I need to send the one byte address with write bit cleared (which RecvBlock() does) prior to receiving the number of bytes specified as a parameter to RecvBlock().
 
Here is the code:
 
   byte error ;
   byte receivedData[4];
   word *bytesRead ;
   destination = port ;   
  
   error = I2C1_SelectSlave( (byte)(destination + ADDRESS_BASE) );
  
   IICCommand.asField.commandByte = INPUT_PORT_REGISTER ;
  
   error = I2C1_SendChar(IICCommand.asField.commandByte);
  
   // blocking while bus is busy
   while(IBSR & IBSR_IBB)  // or while(I2C1_CheckBus())
      PORTE |= 0x04 ;           // for debugging with scope
   PORTE &= ~0x04;     
  
   error = I2C1_RecvBlock(receivedData, 1, bytesRead);
   while(IBSR & IBSR_IBB)
         PORTE |= 0x04 ;
   PORTE &= ~0x04;
  
   *data = receivedData[0] ;   // *data is a parameter to this function
 
I have put a scope on SCL, SDA and on GPIO PE2 and watched this happen over and over. IBB should go high on a start condition and low on a stop condition and indicate a busy bus.
 
 
标签 (1)
0 项奖励
回复
1 回复

954 次查看
NLFSJ
Contributor III
Hi Shawn,
A loss of arbitration, please  read the IIC Phillips spec under LOAs. When there is a loss of arbritation the Master defaults to a Slave and the IBB and other control bits are cleared. To minimize that problem please have the  implement IIC pullup accelarators. Such devices can be found on www.google.comhttp://forums.freescale.com/freescale/board/www.google.com.
I hope this helps.
Regards,
Nina
0 项奖励
回复