I wanna use KITVALVECNTLEVM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I wanna use KITVALVECNTLEVM

1,328 Views
sanghoon_pde
Contributor I


But, I can't configuring the development environment.

How to debug it ?

I try all what I do.

And I have Cyclone FX.

So, I try to debug it.

However I can't know what algorithm I use.

 

I know it's MC9S12XEP100MAL.

But, I can't understand size.

 

153405_153405.pngpastedImage_0.png

 

Please Help me.

I wanna debug my kitvalvecntlevm board.

Labels (1)
0 Kudos
Reply
1 Reply

1,279 Views
iggi
NXP Employee
NXP Employee

Hi,

I suppose you use CodeWarrior v5.1 (or v5.2) for S12(X) MCUs.

There is some issue with the new products of P&E Micro such as Multilink Universal FX and Cyclone FX
Maybe it would be good to contact P&E MIcro support and ask for a device patch:
P&E Microcomputer Systems: Over 30 years as an Industry leader in Embedded Systems Development Tools...

Also, ensure the jumpers on the board are correctly set -> JP1 in 1-2 position (watchdog disabled).

Regards,

iggi

0 Kudos
Reply