I need constant values for 6 pole-pairs(12 poles)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I need constant values for 6 pole-pairs(12 poles)

657 次查看
young-kyunpark
Contributor II

Hi, I'm using MC9S12ZVM and my motor is 6 pole pairs(12pole).

How can I calculates constant values SPEED_CALC_NUMERATOR, STALLCHECK_MIN_CMT_PERIOD, REQUIRED_RUN_SPEED ?

标签 (1)
0 项奖励
回复
1 回复

479 次查看
iggi
NXP Employee
NXP Employee

Hi Park,

First of all, you would need to know motor parameters and start-up parameters from which you can calculate various speeds in Hz and rpm: nominal, max, min, electrical. Then you would need to calculate times and counts (at max speed) for one el. revolution and between two commutations. Also are needed following parameters - voltage to achieve min speed and last start period.

Using this paramaters, by mathematical operations, the constant values are calculated in integer and fractional form.

Regards,

iggi

0 项奖励
回复