Hello Guys,
I have installed Tresos V23.0.0 in order to use it to generate OS code sources for S12Z, I used sample project as example "Os_Sample_Sc1" provided with S12Z_AUTOSAR_OS_4_0_80_RTM_1_0_1P2
I also installed the MCAL S12ZVC_MCAL4_0_RTM_1_0_0
when I try to generate or verify code, the following issues appeared on my screen: (see enclosed screenshot)
Failed to run generator "Os_TS_T34D1M4I0R80GeneratorId" (mode: "verify") for module "Os_TS_T34D1M4I0R80"
do you have any idea about this issue ?
Thank you in advance.
Best Regards,
#
Hello Mohammed,
My colleague meet the same issue with you and after he install the "Java Runtime Environment 5.0 Update 12" in the link Java Archive Downloads - Java SE 5. It work normally.
Best regards,
Hung.
Hello Hung,
I still have the same problem; i add the java folder in my PATH variable environment (see the screenshot) and verified the path using CMD.after a restart, I tried to generate using tresos but I have the same issue.
it's strange ? I think there is another cause of this problem perhaps related to generator of TS_T34D1M4I0R80 ?!
with command when I try to run it, I have the following error
C:\NXP\AUTOSAR\S12Z_AUTOSAR_OS_4_0_80_RTM_1_0_1P2\ssc\bin\generator>sg
Fatal error: Java Runtime Environment 5.0 Update 12 not found
and from the same directory, I can access to Java:
C:\NXP\AUTOSAR\S12Z_AUTOSAR_OS_4_0_80_RTM_1_0_1P2\ssc\bin\generator>java -version
java version "1.8.0_221"
Java(TM) SE Runtime Environment (build 1.8.0_221-b11)
Java HotSpot(TM) Client VM (build 25.221-b11, mixed mode)
BR,
#
Hello Mohammed,
Could you please try to add the "C:\Program Files\Java\jre1.8.0_221" in your PATH variable environment. Cause I have tried:
- Remove the "C:\Program Files\Java\jre1.8.0_221" in my PATH (please see Error.png) and I see that I meet the same issue with you (log.txt)
- After adding the "C:\Program Files\Java\jre1.8.0_221" in my PATH (please see normal.png), the issue is gone.
Note: In my computer I just have JAVA_HOME but not JAVA.
Thank and best regards,
Hung.
Hello Hung,
I don't think that the leading cause is the PATH Environment of JAVA
as you can see below in the screenshot of my CMD the JAVA environment path already set:
so perhaps another cause , do you have any other idea ?
Thanks,
BR,
#
Hello Mohamed,
Currently I cannot reproduce your issue.
Could you please share your file .tresoslog in folder "tresos\workspace\.metadata". It will help for tracing this issue.
Best regards,
Hung.
Hello Mohammed TAOUG,
I guess that you are missing the PATH environment for java.exe. Could you please check it ?
Then please try to open CMD and run the command:
C:\EB\tresos\..\..\NXP\AUTOSAR\S12Z_AUTOSAR_OS_4_0_80_RTM_1_0_1P2\ssc\bin\generator\sg.exe C:\NXP\AUTOSAR\S12Z_AUTOSAR_OS_4_0_80_RTM_1_0_1P2\os_ts\eclipse\workspace\os_sample_sc1\output\epc\project.epc