I USE MOLLOC IN S12G

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I USE MOLLOC IN S12G

1,919件の閲覧回数
wojinandawei
Contributor II

us the tile, I use molloc function sucessfuly in S12G128 mcu。

and this way solve one bug that my code will stop at a  not certern position, because of the use of RAM.

Because , I just use a  buf[384] way for example, and so total RAM size is reduced. 

But after use molloc way, this question is solved .

0 件の賞賛
返信
2 返答(返信)

1,700件の閲覧回数
aaronlee
Contributor V

Hi,

You can refer Array over 123 elements .

Hope it can help you.

Best Regards,

Aaron

タグ(1)
0 件の賞賛
返信

1,702件の閲覧回数
aaronlee
Contributor V

repeat

0 件の賞賛
返信