I USE MOLLOC IN S12G

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I USE MOLLOC IN S12G

1,495 Views
wojinandawei
Contributor II

us the tile, I use molloc function sucessfuly in S12G128 mcu。

and this way solve one bug that my code will stop at a  not certern position, because of the use of RAM.

Because , I just use a  buf[384] way for example, and so total RAM size is reduced. 

But after use molloc way, this question is solved .

0 Kudos
Reply
2 Replies

1,276 Views
aaronlee
Contributor V

Hi,

You can refer Array over 123 elements .

Hope it can help you.

Best Regards,

Aaron

Tags (1)
0 Kudos
Reply

1,278 Views
aaronlee
Contributor V

repeat

0 Kudos
Reply