How to run xCAN driver(AN2726)on the demo board DEMO9S12XDT512?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to run xCAN driver(AN2726)on the demo board DEMO9S12XDT512?

1,665 Views
tranvkhoa
Contributor I
Dear CAN driver and everybody!

Did you run xCAN driver(AN2726)on the demo board DEMO9S12XDT512 successfully? I'm loading this driver into the board but encountering error (pls see attached file).

Do we have to make any modification in order the code to run? I'm using CW 4.6

Thanks,
Khoa
Labels (1)
0 Kudos
2 Replies

365 Views
candriver
Contributor I
Hi...
 
There s no error in ur attach file....it should be work properly on demo board MC9S12XDT512.
0 Kudos

365 Views
Steve
NXP Employee
NXP Employee
There are no errors shown in the attached file. CodeWarrior doesn't find some command files but it looks like it correctly programs your code into the MCU.
 
0 Kudos