How to realize PMSM high load low speed start

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to realize PMSM high load low speed start

1,151 次查看
maxxu
Contributor IV

Hi NXPtechnical team

      I refer to the FOC control application of s912zvm(AN5135). The official scheme, rotor position / speed estimation uses BEMF observer. This principle has requirements on the speed, which is not applicable to the occasion of starting at very low speed with large load.

      I need to be able to use the zero speed control scheme, whether the high-frequency injection method is used, and if the resources of s912zvm cannot be met, Can it be implemented on s32k series chips? I look forward to NXP's application in this regard.

                                                                   Thank you

0 项奖励
回复
0 回复数