How to realize PMSM high load low speed start

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to realize PMSM high load low speed start

1,153 Views
maxxu
Contributor IV

Hi NXPtechnical team

      I refer to the FOC control application of s912zvm(AN5135). The official scheme, rotor position / speed estimation uses BEMF observer. This principle has requirements on the speed, which is not applicable to the occasion of starting at very low speed with large load.

      I need to be able to use the zero speed control scheme, whether the high-frequency injection method is used, and if the resources of s912zvm cannot be met, Can it be implemented on s32k series chips? I look forward to NXP's application in this regard.

                                                                   Thank you

0 Kudos
Reply
0 Replies