How to prevent malfunction of S912ZVC19F0MLF mcu

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to prevent malfunction of S912ZVC19F0MLF mcu

Jump to solution
1,732 Views
s_kim1
Contributor III

Hello,

I made the product using S912ZVC19F0MLF mcu and got the best rating.

I was very happy to find the best mcu.

I have a question.

My product only works with ADC input and PWM output.

I wondered if the product I made could work normally for 10 or 20 years.

1. If the MCU product malfunctions due to external shocks during operation, how is it restored?

2. Is there a possibility that an error in operation may be caused by invading an unused memory address due to a malfunction?

3. If an error occurs, how does the mcu solve it?

4. If there is a sample code that can prevent the error, please provide it.

5. In addition to Watchdog, please tell me how to prevent the error.

We look forward to your response.

thanks.

0 Kudos
Reply
1 Solution
1,718 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello,

You may refer to the S12ZVM Safety Manual that provides guidelines on how to configure and operate the MagniV Safety Devices.

The Safety Manual is available in SafeAssure NDA group

https://community.nxp.com/groups/safeassure-nda

The community is monitored by our expert on application safety.

So, I would recommend posting the questions there.

You would need to have an NDA first as described in this document.

https://community.nxp.com/docs/DOC-335524

 

All the questions are too generic though.

1.
The MCU can be reset by clock monitors or the MCU can detect a machine exception.

2.

danielmartynek_0-1608131836296.png

3 & 4.
Please take a look at this example:
https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12Z-machine-exception-caused-by-ECC-issue-...

5.
I don’t understand this question.
Can you please elaborate?

 

Regards,

Daniel

 

 

 

 

 

 

View solution in original post

0 Kudos
Reply
2 Replies
1,719 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello,

You may refer to the S12ZVM Safety Manual that provides guidelines on how to configure and operate the MagniV Safety Devices.

The Safety Manual is available in SafeAssure NDA group

https://community.nxp.com/groups/safeassure-nda

The community is monitored by our expert on application safety.

So, I would recommend posting the questions there.

You would need to have an NDA first as described in this document.

https://community.nxp.com/docs/DOC-335524

 

All the questions are too generic though.

1.
The MCU can be reset by clock monitors or the MCU can detect a machine exception.

2.

danielmartynek_0-1608131836296.png

3 & 4.
Please take a look at this example:
https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12Z-machine-exception-caused-by-ECC-issue-...

5.
I don’t understand this question.
Can you please elaborate?

 

Regards,

Daniel

 

 

 

 

 

 

0 Kudos
Reply
1,700 Views
s_kim1
Contributor III

5. Ask again about
I want to make an ASIL D rated product.
What is the software part that can be done with S912ZVC19F0MLF product?

 

Thanks.

0 Kudos
Reply