How to prevent malfunction of S912ZVC19F0MLF mcu

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to prevent malfunction of S912ZVC19F0MLF mcu

跳至解决方案
1,847 次查看
s_kim1
Contributor III

Hello,

I made the product using S912ZVC19F0MLF mcu and got the best rating.

I was very happy to find the best mcu.

I have a question.

My product only works with ADC input and PWM output.

I wondered if the product I made could work normally for 10 or 20 years.

1. If the MCU product malfunctions due to external shocks during operation, how is it restored?

2. Is there a possibility that an error in operation may be caused by invading an unused memory address due to a malfunction?

3. If an error occurs, how does the mcu solve it?

4. If there is a sample code that can prevent the error, please provide it.

5. In addition to Watchdog, please tell me how to prevent the error.

We look forward to your response.

thanks.

0 项奖励
回复
1 解答
1,833 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hello,

You may refer to the S12ZVM Safety Manual that provides guidelines on how to configure and operate the MagniV Safety Devices.

The Safety Manual is available in SafeAssure NDA group

https://community.nxp.com/groups/safeassure-nda

The community is monitored by our expert on application safety.

So, I would recommend posting the questions there.

You would need to have an NDA first as described in this document.

https://community.nxp.com/docs/DOC-335524

 

All the questions are too generic though.

1.
The MCU can be reset by clock monitors or the MCU can detect a machine exception.

2.

danielmartynek_0-1608131836296.png

3 & 4.
Please take a look at this example:
https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12Z-machine-exception-caused-by-ECC-issue-...

5.
I don’t understand this question.
Can you please elaborate?

 

Regards,

Daniel

 

 

 

 

 

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,834 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hello,

You may refer to the S12ZVM Safety Manual that provides guidelines on how to configure and operate the MagniV Safety Devices.

The Safety Manual is available in SafeAssure NDA group

https://community.nxp.com/groups/safeassure-nda

The community is monitored by our expert on application safety.

So, I would recommend posting the questions there.

You would need to have an NDA first as described in this document.

https://community.nxp.com/docs/DOC-335524

 

All the questions are too generic though.

1.
The MCU can be reset by clock monitors or the MCU can detect a machine exception.

2.

danielmartynek_0-1608131836296.png

3 & 4.
Please take a look at this example:
https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12Z-machine-exception-caused-by-ECC-issue-...

5.
I don’t understand this question.
Can you please elaborate?

 

Regards,

Daniel

 

 

 

 

 

 

0 项奖励
回复
1,815 次查看
s_kim1
Contributor III

5. Ask again about
I want to make an ASIL D rated product.
What is the software part that can be done with S912ZVC19F0MLF product?

 

Thanks.

0 项奖励
回复