How to improve the efficiency of the controller

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to improve the efficiency of the controller

642 次查看
fanlikang
Contributor II

Dear Expert:

      We have designed a water pump control board according to the program and schematic provided on the official website. The rated power of the water pump is 450w, and after testing, the efficiency of the controller is about 90%. Figure 1 shows the physical image of the controller we designed. But when we were browsing other articles, we found that the same NXP chip water pump chip claimed that their controller efficiency could reach 95%. We felt that this data was unreliable because they all used the same chip and hardware circuit, and the only difference was the selection of MOS. However, the gap was so large. May I ask if there was any problem with their controller data? The picture shows their controller PCB and physical image.

  Best wishes

  Likangfan

0e461e803be1dc3c13ac4c7f036abd8.jpg

                                                     The controller we designed

                      微信截图_20230911113611.png

                                                  We suspect a faulty controller

0 项奖励
回复
0 回复数