How to get the machine code file from a target board with an un-protected or un-secured Flash MCU?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to get the machine code file from a target board with an un-protected or un-secured Flash MCU?

1,354件の閲覧回数
kunxu
Contributor II

Hello, I have a target board with a MC9S12XEP100 chip. The flash of the MCU chip is un-protected and un-secured. I want to get the machine code file or assembly file (*.abs, or *.s19). What should I do?

PS: I have succesfully connected the target board using the BDM (P&E USB Multilink Inerface) via the software - hiwave.exe, and see the contents of the Flash memory, as well as the Assemble codes  in the Windows of "Memory" and "Assemble" of the hiwave.exe software, respectively. But I don't know how to save them as a *.abs file or a *.s19 file.  The copy command cannot be used in the Windows "Memory" or "Assemble" of the hiwave.exe software

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,115件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

hello Kun,

my colleague already provided the answer:

How to get the machine code file from a target board with an un-protected or un-secured Flash MCU?


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,115件の閲覧回数
iggi
NXP Employee
NXP Employee

Jennie, thanks for digging that out :-)

0 件の賞賛
返信

1,115件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

you are welcome!


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信