How to download .S19 file to 9S12 chip when no source code in hand?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to download .S19 file to 9S12 chip when no source code in hand?

3,982件の閲覧回数
lijiandong
Contributor I
I  couldn't found the  program in the Codewarrior for 9S12 to do the .S19 dowloading.
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,264件の閲覧回数
peg
Senior Contributor IV
Ni Hao,
 
to download an s19 file:
start hiwave.exe in the progs dir of your codewarrior installation
under 'Component' menu choose 'select device'
then select your device
when press OK it should connect to the device through your interface.
Then under the menu which is named as per your interface select 'load'
change filetype to .s19 and open your file
Then you should get the erase and programme dialog and your done!
 
Regards Peg
 
0 件の賞賛
返信

1,264件の閲覧回数
lijiandong
Contributor I
thank you ,I will try
0 件の賞賛
返信