How to Enable the PTUT0PE to show the internal trigger_0 event on Pin PS0?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to Enable the PTUT0PE to show the internal trigger_0 event on Pin PS0?

1,134 Views
chenqizhi
Contributor I

Hi,in my application,I use the S12ZVML(F1) to control a PMSM motor . To confirm the sample time, I have set the PTUT0PE to show trigger_0 event by 

PTUDEBUG_PTUT1PE = 1;

PTUDEBUG_PTUT0PE = 1; but I can't get any wave in PS0 and PS1(Pin3 and Pin4)?

(I didn't use CAN function)

Labels (1)
0 Kudos
Reply
2 Replies

1,027 Views
lama
NXP TechSupport
NXP TechSupport

Hi,

is the issue still active?

If yes, do you measure the signal in a normal or a special mode because PTUDEBUG is writeable in the special mode only?

Best regards,

Ladislav

0 Kudos
Reply

1,027 Views
chenqizhi
Contributor I

Didn't I descrip clearly?

0 Kudos
Reply