I've need of 15 PWM output in an application that use S12zvl 64 k microcontroller. 8 outputs are from PWM peripheral. Timer 1 is used for other purpose, so are not available. So I've need of 7 channels from Timer 0. In the Reference manual is written that Timer 0 has 6 channels, but in this link
S12ZVL Mixed-Signal MCU|MagniV|NXP
is written that Timer 0 has 8 channels (and Timer 1 4 channels). (reference manual is attached)
How many channels are available in Timer 0 and Timer 1 for S12ZVL 64,96,128K?
Thank you
Hi,
The reference manual is correct, S12ZVL64/94/128 MCUs have Timer_0 (6ch) and Timer_1(2ch).
The information on the web is not correct, it has been recently reported, it should be fixed.
Regards,
Daniel