How can we set up a 64 - bit Integer operations under  CodeWarrior Development Studio for HCS12(X) Microcontrollers (Classic IDE) v5.1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How can we set up a 64 - bit Integer operations under  CodeWarrior Development Studio for HCS12(X) Microcontrollers (Classic IDE) v5.1

2,871 次查看
xiuminsong
Contributor I

The customers is using CodeWarrior Development Studio for HCS12(X) Microcontrollers (Classic IDE) v5.1 do a S12 project,Which need use 64 bit integer operations. The results is correct when set unsigned long 32 bits, But if set to unsigned longlong 64 bits , the result is error. How can we set up a 64 - bit integer? thanks!

标签 (1)
0 项奖励
回复
5 回复数

2,502 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Xiumin,

When you create project , please try configure :

pastedImage_0.png

Hope it helps


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,503 次查看
xiuminsong
Contributor I

Dear Alice,

Thanks for your reply.

I've tried this, but it's floating point type, and use an integer that needs to change.

Best Regards,

0 项奖励
回复

2,502 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Xiumin,

Sorry  i said before is wrong .

the HCS12(x) chips is 16 bit , so the maximum bit is 32 , it can not  realize 64 bits.

For the kinetis chip , for it is 32 bit , so the longlong type is 64 bits.

Hope it helps


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,503 次查看
kef2
Senior Contributor V

Alice,

It's not true that 16bit MCU can't have 64bit integers in C. Even 8bit MCU's can do. But CW for S12(X) doesn't support it.

0 项奖励
回复

2,503 次查看
xiuminsong
Contributor I

Dear Alice,

Thank you very much!

Best Regards,

0 项奖励
回复