HD PIN isssues for S912ZVML12F1WKH_LQFP64

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HD PIN isssues for S912ZVML12F1WKH_LQFP64

1,041 Views
parker_yu
Contributor I

S912ZVML12F1WKH.png1,帮忙下HD管脚的内部电路,其中分压电阻值是多少?

2,该引脚对输入电流大小的范围为多少?

3,外部分压的这种方式有没有什么风险?(以前12V输入系统的方式是串单颗几十欧姆的电阻)

目前我司用MCU10PIN(HD)做母线电压采样,因为我的是24V系统,所以我在外部用两电阻分压之后再给到HD管脚。

现测试发现,外部分压电阻用的太大时,母线电压采样就会偏差越大。根据调试结果,外部 分压电阻大于1.5K时,母线采样就会开始不准确。

估计是被MCU_HD脚内部为两颗电阻分压了,或者是输入电流太小。

0 Kudos
3 Replies

898 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi parker.yu@arrow.com,

Please write you posts in English.

The specification that you are looking for is in the S12ZVM reference manual, rev.2.13.

pastedImage_2.png

https://community.nxp.com/docs/DOC-341377 

AN5082 MagniV in 24V Applications

AN11967 S12ZVM Family in 48 V Applications

BR, Daniel

0 Kudos

898 Views
parker_yu
Contributor I

Dear Daniel, thanks so much.

0 Kudos

898 Views
parker_yu
Contributor I

Datasheet 没有找到 HD PIN 的输入电阻值的参数。

0 Kudos