Gdu Fault at rpm Variable

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Gdu Fault at rpm Variable

跳至解决方案
2,772 次查看
seunghwan_jeon
Contributor I

The motor was driven based on S12ZVMLMINIBRD_BLDC_SW_CW11.
It runs from 1000 rpm to 3500 rpm.
GDU Fault occurs when RPM is changed by 1 second.
Also added GDU fault clear function.
Charge pump function has also been added.
The reliability test has a variable speed test, but it does not work.
If you know, please help.

0 项奖励
回复
1 解答
2,609 次查看
pachamatej
NXP Employee
NXP Employee

Hello,

can you please be more specific about the situation you are getting the fault?

For example:

Are you using your own motor or the original one?

At which speed does the GDU fault appear?

Which GDU fault specifically do you see? (Use the FreeMASTER and look for _GDUF.byte and _GDUDSE.byte values after the fault occurs)

Please let us know.

Best regards,

Matej

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,610 次查看
pachamatej
NXP Employee
NXP Employee

Hello,

can you please be more specific about the situation you are getting the fault?

For example:

Are you using your own motor or the original one?

At which speed does the GDU fault appear?

Which GDU fault specifically do you see? (Use the FreeMASTER and look for _GDUF.byte and _GDUDSE.byte values after the fault occurs)

Please let us know.

Best regards,

Matej

0 项奖励
回复
2,608 次查看
seunghwan_jeon
Contributor I

Hi Thanks for the answer.
The same error value does not always occur when reading a GDU fault.
Sometimes only GDUF occurs, and sometimes it comes with a GDUDSE error.
Also, GDUDSE or GDUF bytes are different depending on the situation.
I tested it separately, but there is no such phenomenon in a square wave source.
Thank you.

0 项奖励
回复