Flexray with s12xe microcontoller 

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Flexray with s12xe microcontoller 

1,481件の閲覧回数
claudialopresti
Contributor I

Dear,

we'd like to use the flexray bus with the s12xe microcontroller.

Is that possible?

We've seen that exist the MFR4310 used with the S12XD model, could we use the same for the S12XE?

 

Thank you for your help.

 

Sincerelly,

ラベル(1)
3 返答(返信)

1,311件の閲覧回数
iggi
NXP Employee
NXP Employee

Hi,

The S12XE does not have FlexRay module integrated on chip, niether do S12XD. The only chip with that feature is S12XF family (F indicates FlexRay). However, the MFR4310 is the FlexRay communication controller and can be used with S12XE microcontroller.

The EVB9S12XDP512 evaluation board has dedicated part and headers to plug-in the MFR4310FRDC daughter card:

EVB91S12XDP512 Schematics (REV 1.0)

FlexRay™ Daughter Card (FRDC) (MFR4300FRDC)

From the EVB schematic you can see where flexray header pins are routed (to which MCU pins), so you can use the same implementation with S12XE evaluation board which does not have that headers on it.

Hope the information helps.

Regards,

iggi

0 件の賞賛
返信

1,311件の閲覧回数
billkrakar
NXP Employee
NXP Employee

Good question. I will check with our technical team and have them respond.

Bill Krakar

0 件の賞賛
返信

1,311件の閲覧回数
claudialopresti
Contributor I

Hi Bill,

thank you for your response.

Have you finnally checked with your technical team?

Claudia