Finding MCAT Lib on Web of NXP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Finding MCAT Lib on Web of NXP

1,004 Views
ahnjoseph
Contributor III

I received a MCAT FOC LIB(S12zvm) from this site

But I did not find a MCAT FOC Lib on Web NXP

 

I did tri with MCAT LIB source at EVB Kit (MTRCKTSBNZVM128 )

But that was N.G work

So I want to good work MCAT FOC Lib source on MTRCKTSBNZVM128kit

Labels (1)
0 Kudos
Reply
1 Reply

897 Views
iggi
NXP Employee
NXP Employee

Hi,

MCAT tool is not available for download on NXP web as it is not a standalone tool yet. It's rather a plugin for FreeMaster tool. We are working to make it standalone and hopefully this will be available this year.

The MCAT FOC lib you've got should be used with PMSM Motor Control Kit with  MagniV MC9S12ZVM - MTRCKTSPNZVM128.

The kit you are using is for BLDC motor control as indicated by letter B in the part number.

Now i'm not sure if we have the MCAT for the BLDC kit, probably yes. need to check.

Regards,

iggi

0 Kudos
Reply