Error after suspend/breakpoint during debug

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Error after suspend/breakpoint during debug

3,604 次查看
buch2001
Contributor II

Hi all,
I inherited a project to develop and I have a problem with debugging.
When I put a breakpoint (or do "suspend") the software does not resume working properly.
I give an example with the code:
if(locVBatt >= VBATT_MAX_OFF)
{
batSts = BAT_FILT_OVERV;
vCnt++;
}
else if(locVBatt <= VBATT_MIN_OFF)
{
batSts = BAT_FILT_UNDERV;
vCnt++;
}
else
{
vCnt = RESET;
}
I put a breakpoint inside the first "if" (let's say it's "true"), then restart code execution. The brekpoint continues to run ad always enters the first branch.
Then I move the brekpoint into the "else if", change the conditions so that it is "true" but never enters the "else if" but continues to enter the first "if".

Obviously if I create the conditions that it is true the "else if" at the first execution works correctly.

Same thing if instead of a brekpoint I make a normal "suspend" during the run.
It just seems that the software does not resume working properly, I have never seen such behavior and I really don't know how to fix it.

Thank you very much to those who can help me

 

0 项奖励
回复
9 回复数

3,596 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @buch2001,

Can you specify the MCU, IDE and the debug probe?

 

Thank you,

BR, Daniel

0 项奖励
回复

3,595 次查看
buch2001
Contributor II

Sure, sorry.

I'm using MC9S12ZVMARM, the IDE is CodeWarrior and I'm debugging via Multilink universal

0 项奖励
回复

3,588 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Have you tried updating the PE Micro Multilink drivers

danielmartynek_0-1674554561327.png

 

and the firmware of the probe?

https://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320180&productTab=4

danielmartynek_1-1674555254471.png

danielmartynek_2-1674555315697.png

 

 

0 项奖励
回复

3,585 次查看
buch2001
Contributor II

I did but nothing changed. 

There seems to be some configuration options, but I don't know which ones....

 

I just add a little information that might be helpful:

Looking at the previous code example (I put numbers), the starting condition is the following:

buch2001_2-1674557185676.png

buch2001_3-1674557224191.png

so putting a brekpoint it enters in the correct branch.

 

Then

 

if I try to change the value of the variable AFTER stopping the code with a breakpoint and advancing step-by-step the software seems to ignore the new value and continues to enter the previous branch:

buch2001_4-1674557628257.png

buch2001_5-1674557641881.png

 

buch2001_0-1674557065148.png

buch2001_6-1674557675881.png

 

0 项奖励
回复

3,577 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

I'm not able to reproduce it.

Does the variable change in the memory view?

Can you read it in the memory before the condition is executed?

Is it a global variable or is it on the stack?

 

 

0 项奖励
回复

3,573 次查看
buch2001
Contributor II

after some analysis it seems to me that it is the adc that stops working. But I really can't understand why

0 项奖励
回复

3,561 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Marco,

I'm not sure what you mean, and how it is related to the original issue.

Where are the ADC commands stored?

Do you see any ADC error (ADCEIF)?

 

BR, Daniel

 

0 项奖励
回复

3,556 次查看
buch2001
Contributor II

At the end of my investigation it seems that the whole problem stems from the fact that the Autonomous Periodic Interrupt continues to be active during debugging, triggering its interrupt when time expires and then setting an internal error that resets some variables.
Now we are a bit off topic from the original topic, but is it possible to disable it during debugging?

 

In my debug coonfiguration I've set this option, I hoped was enough

buch2001_0-1674725998335.png

 

0 项奖励
回复

3,550 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Yes, this disables it during the stepping through the code, but not while you are debugging.

It should be disabled by default though.

Was it enabled in your original configuration?

 

When you let the code run without stepping, doesn't the API overwrite the variables too?

 

You can disable the API interrupt at the first breakpoint by writting to the (CPMUAPICTL_APIE = 0) register via the debugger.

 

0 项奖励
回复