Error:  C2450: Expected:  ~ ( IDENT    MC9S12XEP100.h line 1799

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error:  C2450: Expected:  ~ ( IDENT    MC9S12XEP100.h line 1799

2,034 Views
mikoran
Contributor II
Hi.
Can you help me how to deal with this error?
I have this code below in my MC9S12XEP100.h file and during compilation I have an error pointed to the highlighted line. Please help me with this..
 
 
/*** DBGTB - Debug Trace Buffer Register; 0x00000024 ***/
typedef union {
  word Word;
   /* Overlapped registers: */
  struct {
    /*** DBGTBH - Debug Trace Buffer Register High; 0x00000024 ***/
    union {
      byte Byte;
      struct {
        byte BIT8        :1;
        byte BIT9        :1;  
        byte BIT10       :1;  
        byte BIT11       :1; 
        byte BIT12       :1;
        byte BIT13       :1;    
        byte BIT14       :1; 
        byte BIT15       :1;
      } Bits;
    } DBGTBHSTR;
    #define DBGTBH                      _DBGTB.Overlap_STR.DBGTBHSTR.Byte
    #define DBGTBH_BIT8                 _DBGTB.Overlap_STR.DBGTBHSTR.Bits.BIT8
    #define DBGTBH_BIT9                 _DBGTB.Overlap_STR.DBGTBHSTR.Bits.BIT9
    #define DBGTBH_BIT10                _DBGTB.Overlap_STR.DBGTBHSTR.Bits.BIT10
    #define DBGTBH_BIT11                _DBGTB.Overlap_STR.DBGTBHSTR.Bits.BIT11
    #define DBGTBH_BIT12                _DBGTB.Overlap_STR.DBGTBHSTR.Bits.BIT12
    #define DBGTBH_BIT13                _DBGTB.Overlap_STR.DBGTBHSTR.Bits.BIT13
    #define DBGTBH_BIT14                _DBGTB.Overlap_STR.DBGTBHSTR.Bits.BIT14
    #define DBGTBH_BIT15                _DBGTB.Overlap_STR.DBGTBHSTR.Bits.BIT15
    
    #define DBGTBH_BIT8_MASK            1
    #define DBGTBH_BIT9_MASK            2
    #define DBGTBH_BIT10_MASK           4
    #define DBGTBH_BIT11_MASK           8
    #define DBGTBH_BIT12_MASK           16
    #define DBGTBH_BIT13_MASK           32
    #define DBGTBH_BIT14_MASK           64
    #define DBGTBH_BIT15_MASK           128

    /*** DBGTBL - Debug Trace Buffer Register Low; 0x00000025 ***/
    union {
      byte Byte;
      struct {
        byte BIT0        :1; 
        byte BIT1        :1;
        byte BIT2        :1; 
        byte BIT3        :1; 
        byte BIT4        :1; 
        byte BIT5        :1; 
        byte BIT6        :1;
        byte BIT7        :1;
      } Bits;
    } DBGTBLSTR;
    #define DBGTBL                      _DBGTB.Overlap_STR.DBGTBLSTR.Byte
    #define DBGTBL_BIT0                 _DBGTB.Overlap_STR.DBGTBLSTR.Bits.BIT0
    #define DBGTBL_BIT1                 _DBGTB.Overlap_STR.DBGTBLSTR.Bits.BIT1
    #define DBGTBL_BIT2                 _DBGTB.Overlap_STR.DBGTBLSTR.Bits.BIT2
    #define DBGTBL_BIT3                 _DBGTB.Overlap_STR.DBGTBLSTR.Bits.BIT3
    #define DBGTBL_BIT4                 _DBGTB.Overlap_STR.DBGTBLSTR.Bits.BIT4
    #define DBGTBL_BIT5                 _DBGTB.Overlap_STR.DBGTBLSTR.Bits.BIT5
    #define DBGTBL_BIT6                 _DBGTB.Overlap_STR.DBGTBLSTR.Bits.BIT6
    #define DBGTBL_BIT7                 _DBGTB.Overlap_STR.DBGTBLSTR.Bits.BIT7
    
    #define DBGTBL_BIT0_MASK            1
    #define DBGTBL_BIT1_MASK            2
    #define DBGTBL_BIT2_MASK            4
    #define DBGTBL_BIT3_MASK            8
    #define DBGTBL_BIT4_MASK            16
    #define DBGTBL_BIT5_MASK            32
    #define DBGTBL_BIT6_MASK            64
    #define DBGTBL_BIT7_MASK            128
  } Overlap_STR;
  struct {
    word BIT0        :1;
    word BIT1        :1;
    word BIT2        :1; 
    word BIT3        :1;
    word BIT4        :1;  
    word BIT5        :1; 
    word BIT6        :1;
    word BIT7        :1;
    word BIT8        :1; 
    word BIT9        :1; 
    word BIT10       :1; 
    word BIT11       :1; 
    word BIT12       :1; 
    word BIT13       :1;
    word BIT14       :1;
    word BIT15       :1; 
  } Bits;
} DBGTBSTR;
extern volatile DBGTBSTR _DBGTB @(REG_BASE + 0x00000024);
#define DBGTB                           _DBGTB.Word
#define DBGTB_BIT0                      _DBGTB.Bits.BIT0
#define DBGTB_BIT1                      _DBGTB.Bits.BIT1
#define DBGTB_BIT2                      _DBGTB.Bits.BIT2
#define DBGTB_BIT3                      _DBGTB.Bits.BIT3
#define DBGTB_BIT4                      _DBGTB.Bits.BIT4
#define DBGTB_BIT5                      _DBGTB.Bits.BIT5
#define DBGTB_BIT6                      _DBGTB.Bits.BIT6
#define DBGTB_BIT7                      _DBGTB.Bits.BIT7
#define DBGTB_BIT8                      _DBGTB.Bits.BIT8
#define DBGTB_BIT9                      _DBGTB.Bits.BIT9
#define DBGTB_BIT10                     _DBGTB.Bits.BIT10
#define DBGTB_BIT11                     _DBGTB.Bits.BIT11
#define DBGTB_BIT12                     _DBGTB.Bits.BIT12
#define DBGTB_BIT13                     _DBGTB.Bits.BIT13
#define DBGTB_BIT14                     _DBGTB.Bits.BIT14
#define DBGTB_BIT15                     _DBGTB.Bits.BIT15
Labels (1)
0 Kudos
1 Reply

357 Views
CompilerGuru
NXP Employee
NXP Employee
Whenever you have such a kind of strange error, you should check the preprocessor output.
In your particular case I guess somewhere in your code, there is a define for BIT0,
something like

#define BIT0 1

Daniel
0 Kudos