ESD testing failure for MC9S12XET256MAG

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ESD testing failure for MC9S12XET256MAG

1,021件の閲覧回数
kumara
Contributor I

we are using the controller MC9S12XET256MAG for our transmission ECU. While doing ESD test(Air discharge) near controller area, the controller is getting halt during the exposure.It's recovering only after the hard reset of the device. Kindly suggest some solution to rectify the same.

タグ(1)
0 件の賞賛
返信
2 返答(返信)

889件の閲覧回数
chithanhhoang
Contributor II

I have the same problem on the LS1043A chip, my work around is to program the hw watchdog to reset if the cores are frozen because of ESD.

Not the ideal solution but work for me.

Hope my comment helps you.

0 件の賞賛
返信

953件の閲覧回数
lama
NXP TechSupport
NXP TechSupport

Hi,

standard procedure.....

1) Could you please send a readable schematic of the MCU environment?

2) Also good to see whether PCB is OK especially all unused pins correctly (https://www.nxp.com/docs/en/application-note/AN3262.pdf ), no wire or plane under oscillator circuitry, correctly calculated load capacitances,.....

Best regards,

Ladislav

0 件の賞賛
返信