EEPROM Erase time

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,934件の閲覧回数
jingfang
Contributor IV

I am using S12zvl 128ms, It is taking 5.04ms to erase one sector (4 Bytes) on EEPROM.

If I want to erase 64 bytes, how long will it take me?

Is it 64/4*5ms?

Is there another way to speed things up?

0 件の賞賛
返信
1 解決策
1,928件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @jingfang,

There is only the specification that can be found in the RM, Table E-2.

The execution time depends on f_NVMOP and f_NVMBUS (footnotes 1-4).

4.80ms is then the minimum for 4B sector.

And ~((64 / 4) * 4.8ms) for 64 bytes.

 

BR, Daniel 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,929件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @jingfang,

There is only the specification that can be found in the RM, Table E-2.

The execution time depends on f_NVMOP and f_NVMBUS (footnotes 1-4).

4.80ms is then the minimum for 4B sector.

And ~((64 / 4) * 4.8ms) for 64 bytes.

 

BR, Daniel 

0 件の賞賛
返信