Dual S12x Communication

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Dual S12x Communication

1,183 次查看
rayhall
Contributor V

I am thinking of a new product that uses two S12XE. One MCU will be a slave and read sensors. The main MCU would either request the information from the slave or receive it when is ready. I have done this in the past using SCI. I am looking at using CAN Bus to communicate.  Do I still need CAN transceivers, or can I just connect the low level signals from the CAN pins.

 

I am open to ideas using some other method.

 

Ray.

标签 (1)
0 项奖励
回复
2 回复数

1,001 次查看
RadekS
NXP Employee
NXP Employee

Hi Ray,

Edward is right.

You don’t need transceivers. For short length communication, diodes and pull-up are sufficient solution.

Here is simply scheme for connection of four CAN modules together at DEMO9S12XEP100 board as inspiration for you:

CAN without transceiver DemoXEP100.bmp

Tested and proved.


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,001 次查看
kef2
Senior Contributor V
0 项奖励
回复