Our customer has a request on our bootloader, that is, the flash diver must not stored into the flash, it should download from can cummunication and then excute it to do flash download operation. I had noted that our community have some question about how to excute a function on ram, but they were all store into the flash, and when needed or program start, copy to ram, they are still store in flash. what I need is when: excute compile, I can get a section of target file in ram. not place in flash. and i have tried to do this, so I modified the prm file: use the ram as read-only type and place function in it, but I couldn't find any code in the ram place in the s19 file.
The test main.c is like this:
#include <hidef.h> /* common defines and macros */
#include "derivative.h" /* derivative-specific definitions */
#define TEST_OLD PT1AD_PT1AD3
#define TEST_TEMP PTR_PTR4 
#define TEST_NEW PORTB_PB3
#define TEST_IO TEST_NEW
#pragma CODE_SEG ROM_INTO_RAM2 
void Test(void)
{
 static volatile unsigned int test_cnt;
 
 test_cnt ++;
 if (test_cnt > 40000)
 {
 test_cnt = 0;
 TEST_IO = TRUE;
 }
 /*TEST_IO = FALSE;*/
}
#pragma CODE_SEG DEFAULT 
 
void main(void) 
{
 /* put your own code here */
 unsigned int cnt2;
 EnableInterrupts;
 
 DDR1AD_DDR1AD3 = TRUE;
 DDRR_DDRR4 = TRUE;
 DDRB_DDRB3 = TRUE;
 
 for(;;) 
 {
 Test();
 
 if (cnt2 ++ > 30000)
 {
 cnt2 = 0;
 TEST_IO = FALSE;
 }
 _FEED_COP(); /* feeds the dog */
 } /* loop forever */
 /* please make sure that you never leave main */
}
and the prm file is as below:
/* This is a linker parameter file for the MC9S12HY64 */
NAMES END /* CodeWarrior will pass all the needed files to the linker by command line. But here you may add your own files too. */
SEGMENTS /* Here all RAM/ROM areas of the device are listed. Used in PLACEMENT below. */
/* Register space */
/* IO_SEG = PAGED 0x0000 TO 0x03FF; intentionally not defined */
/* RAM */
 RAM = READ_WRITE 0x3000 TO 0x3EFF;
 
 RAM2 = READ_ONLY 0x3F00 TO 0x3FFF;
/* D-Flash */
 DFLASH = READ_ONLY 0x010400 TO 0x0113FF;
/* non-paged FLASHs */
 ROM_1400 = READ_ONLY 0x1400 TO 0x2FFF;
 ROM_4000 = READ_ONLY 0x4000 TO 0x7FFF;
 ROM_C000 = READ_ONLY 0xC000 TO 0xFEFF;
 /* VECTORS = READ_ONLY 0xFF00 TO 0xFFFF; intentionally not defined: used for VECTOR commands below */
 //OSVECTORS = READ_ONLY 0xFF80 TO 0xFFFF; /* OSEK interrupt vectors (use your vector.o) */
/* paged FLASH: 0x8000 TO 0xBFFF; addressed through PPAGE */
 PAGE_0C = READ_ONLY 0x0C8000 TO 0x0C93FF;
 PAGE_0C_B000 = READ_ONLY 0x0CB000 TO 0x0CBFFF;
 PAGE_0E = READ_ONLY 0x0E8000 TO 0x0EBFFF;
/* PAGE_0D = READ_ONLY 0x0D8000 TO 0x0DBFFF; not used: equivalent to ROM_4000 */
/* PAGE_0F = READ_ONLY 0x0F8000 TO 0x0FBEFF; not used: equivalent to ROM_C000 */
END
PLACEMENT /* here all predefined and user segments are placed into the SEGMENTS defined above. */
 _PRESTART, /* Used in HIWARE format: jump to _Startup at the code start */
 STARTUP, /* startup data structures */
 ROM_VAR, /* constant variables */
 STRINGS, /* string literals */
 VIRTUAL_TABLE_SEGMENT, /* C++ virtual table segment */
 //.ostext, /* OSEK */
 NON_BANKED, /* runtime routines which must not be banked */
 COPY /* copy down information: how to initialize variables */
 /* in case you want to use ROM_4000 here as well, make sure
 that all files (incl. library files) are compiled with the
 option: -OnB=b */
 INTO ROM_C000/*, ROM_1400, ROM_4000*/;
DEFAULT_ROM INTO PAGE_0C, PAGE_0C_B000, PAGE_0E;
 
 ROM_INTO_RAM2 INTO RAM2;
 //.stackstart, /* eventually used for OSEK kernel awareness: Main-Stack Start */
 SSTACK, /* allocate stack first to avoid overwriting variables on overflow */
 //.stackend, /* eventually used for OSEK kernel awareness: Main-Stack End */
 DEFAULT_RAM INTO RAM;
//.vectors INTO OSVECTORS; /* OSEK */
END
ENTRIES /* keep the following unreferenced variables */
 /* OSEK: always allocate the vector table and all dependent objects */
 //_vectab OsBuildNumber _OsOrtiStackStart _OsOrtiStart
END
STACKSIZE 0x100
VECTOR 0 _Startup /* reset vector: this is the default entry point for a C/C++ application. */
//VECTOR 0 Entry /* reset vector: this is the default entry point for an Assembly application. */
//INIT Entry /* for assembly applications: that this is as well the initialization entry point */
没有,现在公司的其他人已经搞出来了,我就没再深入,大致就是编译成地址无关代码的方法
prayer_hong@163.com
Hi,
The data are always downloaded into Flash and then copied to RAM during startup.
The data would be lost after power-on reset.
Regards,
Daniel