Does the S9S12XS256J0MAER support BSDL?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does the S9S12XS256J0MAER support BSDL?

536 Views
maximilianweiss
Contributor I

Does the S9S12XS256J0MAER Support BSDL. I need an BSDL-File for the Controller.

Labels (1)
0 Kudos
1 Reply

470 Views
RadekS
NXP Employee
NXP Employee

Hi Maximilian,

S12 devices do not use JTAG interface. Therefore I am afraid that we do not provide BSDL file for S12XS MCUs.

S12XS MCUs are programmed and debugged trough BDM interface.


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos