Does the S912ZVC64F0VLF have CAN PHY built in?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does the S912ZVC64F0VLF have CAN PHY built in?

784 Views
ahnjoseph
Contributor III

Does the S912ZVC64F0VLF have CAN PHY built in?

 

My customer has inform that  s12zvc 256Kb has just CAN PHY 

 Let me know it ...  

0 Kudos
3 Replies

719 Views
RadekS
NXP Employee
NXP Employee

Hi Ahn Joseph,

just single letter misunderstanding in part number:

  • All derivatives from the S12ZVC family have CAN PHY integrated. Target applications: CAN sensors.
  • Only S12ZVMC256 derivative from S12ZVM family has CAN PHY integrated. Target applications: 3ph motor control.

I hope it helps you.

BR

Radek

0 Kudos

717 Views
ahnjoseph
Contributor III

HI

Thanks …. I had update to customer

Best Regards,

Joseph Ahn 安延洙

Staff Field Application Egineer

12th Floor,

KBS Media Center

45,Maebongsan-ro

Mapo-Gu, Seoul, Korea

O +822.6277.6330

M +821053868985

F +822.761.2133

0 Kudos

717 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello,

Yes, the S12ZVC family has a version with an on-chip CAN physical transceiver.

I'm not sure, what do you mean by 256 KB?

See image from the RM rev 2.1

pastedImage_2.png

Best regards,

Diana

0 Kudos