The DEVKIT platform
The NXP released new board platform for automotive products – DEVKIT.
The DEVKIT is a low-cost development platform with Arduino UNO/Mega pin compatibility. In my review, I will focus mainly on DEVKIT-ZVL128 board.
The DEVKIT boards are similar to FRDM boards, but they are slightly wider (58mm versus 53mm) due to moving MCU specific pins to external rows of Arduino pin compatible connectors. So, we should be able to access MCU specific pins even when we connect any Arduino shield on top of this board.
The other currently or soon available DEVKIT boards are:
DEVKIT-MPC5744P
DEVKIT-COMM - 6 LIN and 4 CAN transceivers shield
DEVKIT-MOTORGD – three-phase motor control shield with GD3000 N-channel MOSFETs driver and power stage
Note: The FRDM-KEA boards belongs also into the DEVKIT platform despite on the “FRDM” in the board name.
The Content
What you will get for US$35 (current price on NXP web pages):
The sticker on the box points to the NXP web pages for downloading more documents such as the quick start guide, schematic, PCB BOM and design files, code examples or buy the same board again ;-).
Unfortunately, the board User Guide is not available yet.
This web page is also offering “Getting Started” tab with the interactive quick start guide – quite useless feature since the page forgets on necessary 12V power supply for MCU powering and it proposes old CW5.1 (Classic IDE) for S12(X) instead of CW10 (Eclipse IDE).
What else you will need:
The Board
DEVKIT-ZVL128 board is assembled by:
The great thing is that the board has connector pins named from the bottom side of the PCB = less tracking on schematic.
On another side, some of the MCU pins may be routed to Arduino connectors trough zero Ohm resistors. Since these resistors are very small (size 0402), the potential re-routing will need a solid hand.
It is great that loop type test points arrived finally also on low-cost development boards – now in surface mount version. The small loops may be simply locked by test hooks and measured by laboratory equipment.
The MCU
The S12ZVLA128 is one of MagniV family MCUs using the 180nm NVM + UHV technology that offers the capability to integrate 40V analog components. It integrates S12Z core, features from the existing S12 portfolio together with “high-voltage” analog modules, including the voltage regulator (VREG) and a Local Interconnect Network (LIN) physical layer (LIN PHY).
The S12ZVL(A)128/96/64 derivatives introduces several unique enhancements in comparison with older S12ZVL32/S12ZVL16 derivatives:
I am going to use the PGA for thermocouple measurement in the near future.
Software
The Software Integration Guide guides us through CW 10.6.4 installation and creating a new project with Processor Expert (PE) tool. Unfortunately, while following that guide, I discovered that the CW10.6.4 does not offer PE as an option (only project without PE) when I tried to create an S12ZVL128 project. But this option is available in newer CW10.7 version.
Note: If S12ZVL(A)128 derivative is missing in your CW10.6.4 IDE, please update your CW IDE via menu-Help-Install New Software-FSL MCU Eclipse Update Site and focus mainly on “S12Z Support” and “MCU 10.6.4 Updates” folders.
The code examples contains three primitive example projects:
DEVKIT-ZVL128_Lab1GPIO – configure GPIO pins
DEVKIT-ZVL128_Lab2ADC – initialize and measure ADC value
DEVKIT-ZVL128_Lab3PWM – configure voltage regulator, initialize CLOCK, initialize and measure ADC value, generate PWM
Note: The zip file contains already built projects. The loading it into MCU does not work due to different paths. We have to clean it and build again in our workspace prior loading into the MCU.
These projects are really simple, but they omit some specific potential issues.
For example:
volatile unsigned char adc0_cmdlist[1][4] __attribute__ ((aligned (4))) = {0xC0,0xD0,0xA0,0x00};
volatile unsigned short adc0_results[1] __attribute__ ((aligned (4)));
The NXP offers for this MCU also LIN2.x and SAE J2602 Stack and S12Z NVM Standard Software Driver (Flash/EEPROM driver).
There are also well-documented example codes at Community from Technical support team which may be used for an inspiration. For example:
S12ZVM clock module and PLL configuration - SW examples
S12Z Interrupt catcher for unexpected interrupts
A Library of Functions for HD44780 Based LCD Modules (no R/W) for S12Z devices
S12ZVL-TIM-FrequencyMeasurement
…
The next source of information may be NXP application notes. For example:
AN4723 S12Z MagniV Bootloader with SW,
AN4731 Understanding Injection Current on Freescale Automotive Microcontrollers,
AN4841 S12ZVL LIN Enabled Ultrasonic Distance Measurement with SW,
AN4842 S12ZVL LIN Enabled RGB LED Lighting Application with SW,
AN5084 Hardware Design Guidelines for S12ZVL Microcontrollers,
AN5122 Using Freescale’s LIN Driver with the MagniV Family with SW
Summary
One of the best advantages of DEVKIT platform is the price. When we compare DEVKIT board prices with alternative evaluation boards (if any exist), we may save between 40 and 95 % EVB price depending on target MCU family. For example, the older TRK-S12ZVL board (assembled by S12ZVL32) is bigger, additionally offers 9 user switches, buzzer, HVI potentiometer, switchable LIN_OUT connector and header ring with all MCU pins. But the price is also almost three times higher than the price of DEVKIT-ZVL128.
Also, the connectors with standard 100mils pitch are definitely plus in comparison with previously used TWRPI/PCI EXPRESS connectors and the board allows using plenty of available Arduino shields without complex hardware interconnections. You may look for it for example at Arduino pages, shieldlist.org, Adafruit, …
From my side - thumbs up :smileycheck:.
Hi
One of the customer want to get the DEVKIT-MCSHIELD.
I notice that "Note: The grayed names are just for prototype boards, the final board names may be different."
I am not sure if that board has another name: DEVKIT-MOTORGD. Since it look like the same.
Would you please tell me where can the customer get DEVKIT-MCSHIELD?
Thank you for the help in advance!
Best Regards,
Robin
Hi,
You mention a "12V DC power supply (3.8V~40V) with barrel connector (6mm outside diameter x 2mm inside diameter)" is needed. Can the board also be powered by USB?
My guess is yes as the schematic shows a 'Power Supply Selection section with jumper option to P5V_SWUSB' .
Therefore I tried setting the jumper 13 between 2-3 but no connection 'Target MCU is not responding'. Measuring their is no power on J13 Pin3. This makes me believe MIC2026-1YM is not enabling OUTB because ENB is not powered. (Measuring proves this hypothesis). Why is +VTRG_ENB not enabled by MC9S08JM60CGTE?
Or am I misunderstanding jumper 13?
Hi Peter,
Unfortunately, the DEVKIT-ZVL128 board cannot be directly powered from USB.
The assembled S12ZVL128 MCU is part of MagniV family which is designed for powering directly from 12V line. So, the 5V from USB is simply not sufficient for MCU powering.
Note: The S12ZVL128 MCU may be theoretically directly powered from 5V power supply connected to the VDDX/VDDA pin (MCU is not designed for such use). However, in such case we must connect also VSUP pin the same power line for avoiding any issue with transient effects. Such connection will also disable main features of this MCU(integrated power supply, internal LIN PHY,…)
Yes, the 'Power Supply Selection section with jumper option to P5V_SWUSB' is just misunderstanding.
The jumper J13 (+JP1) choose one of source power supplies (MCU, USB, U13 voltage regulator) only for on-board CAN transceiver and Arduino-Uno compatible J3 header. The output from J13 jumper is P5V0 signal.
I hope it helps you.
Best reagrds
Radek
Hello Radek,
Thanks for the clear explanation.
Do you know if this is somewhere documented?
I have found the quick-reference-guide/DVKITZVL128QSG.pdf but this only suggests the opposite:
"CAUTION:
Hi Peter,
Thank you for notification. I reported this issue almost two years ago.
It seems, that nobody fixed it until now.
I will report it again.
The issue is related to QSG and Getting Started page also …
There is just simple Note on the board web page “12V (1 Amp) power supply is required for debugging and CAN/LIN communication, this is not included in the kit”
Best regards
Radek