DEVKIT-S12XE board power supply tolerances

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DEVKIT-S12XE board power supply tolerances

Jump to solution
404 Views
s_kim1
Contributor III

I purchased the DEVKIT-S12XE to review the S12XE MCU.
I will apply external power to DEVKIT-S12XE.
I have a 12V DC 5A power source.
Please tell me the Power Supply specifications of DEVKIT-S12XE.
Please let me know if I can use 12V 5A DC Output power for DEVKIT-S12XE's board.

Thanks.

Tags (3)
0 Kudos
Reply
1 Solution
392 Views
lama
NXP TechSupport
NXP TechSupport

Hi,

The power supply can be selected from USB or from external source via SBC chip. See jumper J10 for source and J13 for level of supply voltage for MCU.

lama_0-1708514008093.png

 

If you use SBC chip to supply the board then the VSUP is given by characteristic of MCZ33903CD5EK. The data sheet of the device states.

lama_1-1708514008093.png

 

So 12V 5A supply is absolutely OK.

Best regards,

Ladislav

View solution in original post

1 Reply
393 Views
lama
NXP TechSupport
NXP TechSupport

Hi,

The power supply can be selected from USB or from external source via SBC chip. See jumper J10 for source and J13 for level of supply voltage for MCU.

lama_0-1708514008093.png

 

If you use SBC chip to supply the board then the VSUP is given by characteristic of MCZ33903CD5EK. The data sheet of the device states.

lama_1-1708514008093.png

 

So 12V 5A supply is absolutely OK.

Best regards,

Ladislav